Technical FAQs

Ask a Question

What is the Flashing C on the ATV21 and ATV212 drives?

Display is flashing "C"

Product Line:
ATV212, ATV21

All Models and serial numbers

Motor is drawing excessive current or the motor settings in the drive are incorrect.

Flashing C means the drive is in a current limit state.  Check F601 current limit setting it should be set to 1.1X your Drives Full load amps. Typ needs to be set to 2 uLu needs to be motor volage 460vac AU1 = 0 auto ramp off Run the motor if the motor is still pulling excessive current check rotation. Drop the motor leads and megger to the motor with a 1KV megger.
Was this helpful?
What can we do to improve the information ?