Technical FAQs

Ask a Question

When you purchase a ZB2SZ3 how many do you receive?

Issue:
How many ZB2SZ3 Hole Plugs are included in ZB2SZ3?

Product Line:
Operator Interface Push Buttons

Enviroment:
NEMA 1, 3R, 4,12
IP54, 55 56

Cause:
Order System is not clear on package quantity 

Resolution:
One hole plug, they must be purchased in multiples of 10.
Was this helpful?
What can we do to improve the information ?