Technical FAQs

Ask a Question

What are the dimensions for the XAPG39203 Enclosure?

Issue:
Dimensions for a XAPG39203 Enclosure

Product Line:
22mm PUSH Button Enclosures

Environment:
NEMA1, 4,12, 13

Cause:
Not in the Product Digest

Resolution:
It is  6.90" H x 3.15" W s 2.03" D,  3 holes drilled die cast enclosure, 1.58" centerline spacing of hole for vertical mount.
Was this helpful?
What can we do to improve the information ?