Technical FAQs

Ask a Question

Can the ATV21/ATV212 VIA be setup for 0-10V speed and terminal control for start/stop?

Yes,
Check that VIA switch is on voltage
Program TYP to 2 for 60 Hz setting for UL, FH, uL.
FNOD: 1
CNOD: 0
0-10V wire on VIA and CC
Was this helpful?
What can we do to improve the information ?