Technical FAQs

Ask a Question

Can the differential setting be changed to 3 PSI on a 9016GVG1J09?

Issue
Can the differential setting be changed to 3 PSI on a 9016GVG1J09?

Product Line
vacuum switches

Environment
9016GV

Cause
Adjustment

Resolution
This is not possible with the 9016GVG.  Miimum differential is 5 psi.
Was this helpful?
What can we do to improve the information ?