Technical FAQs

Ask a Question

Where can I find a replacement Heatsink fan for my obsolete ATV58 or ATV66 series drive?

Issue:
Where can I find a replacement Heatsink fan for my obsolete ATV58 or ATV66 series drive?

Product Line:
ATV58 and ATV66

Environment:
All

Cause:
Fan has failed and is no longer offered as a repair part.

Resolution:
Customers have had good success using Digikey equivalent fans in our ATV58 and ATV66 series drives.   Contact Digikey at 1-800-344-4539 and have available the original manufacturer and model number from the fan itself.  They can usually cross reference the fan and provide an equivalent replacement.
Was this helpful?
What can we do to improve the information ?