Technical FAQs

Ask a Question

Are the HOMT2020 considered a Thermal-Magneitc breaker?

ISSUE
Are the HOMT2020 considered a Thermal-Magneitc breaker?

PRODUCT LINE
Square D Homeline

ENVIRONMENT


CAUSE


RESOLUTION

Yes, the HOM breakers which includes the tandem are all Thermal-Magneitc breakers .
Was this helpful?
What can we do to improve the information ?