Technical FAQs

Ask a Question

What is the difference between a 2510KO2C and 2510KO6C non-reversing starter?

The 2510KO2C has a 2HP@115VAC - 7.5HP@230VAC - 10HP@460/575VAC  horsepower rating at 3 phase
The 2510KO6C has a 2HP@115VAC - 7.5HP@230VAC - 15HP@460VAC  -20HP@/575VAC horsepower rating at 3 phase.


CTA-ID : 2062344
Was this helpful?
What can we do to improve the information ?