Technical FAQs

Ask a Question

What is the replacement drive part number for a 30 HP VT drive unit @ 480 Volt?

The replacement VFD is the ATV61HD22N4.  
If the VFD is used in an M FLEX, E FLEX, 18 pluse or an MCC, the replacement VFD is the ATV61HD18N4 will need to be changed to IP00

CTA-ID : 2063056
Was this helpful?
What can we do to improve the information ?