Technical FAQs

Ask a Question

What are the adjustment ranges for the dials on an ATSU01N2..LT?

For both the START TIME and STOP TIME dials, setpoint A is 1second and setpoint E is 10seconds.  There is a linear relationship from A to E setpoints.
For the INITIAL VOLTAGE dial, setpoint A is 30% and setpoint E is 80% of full voltage.  There is a linear relationship from A to E setpoints.



CTA-ID : 2061385
Was this helpful?
What can we do to improve the information ?