Technical FAQs

Ask a Question

What are the repair parts for a HOM30M150RB, Series S02, load center?

Issue:
Previous design repair parts

Product Line:
Homeline load center

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4056317450 (Includes hinges attached to left side of cover)
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056313802K (ObSOLETE NO LONGER AVAILABLE - ORDER 4056313801K)
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - HOM30M150RBI
Main Breaker - QOM2150VH
Neutral Bonding Screw - 4028345850K
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2044121
Was this helpful?
What can we do to improve the information ?