Technical FAQs

Ask a Question

What are the catalog numbers for the field-installable undervoltage (UVR) accessories for Powerpact DG, DJ, and DL type circuit breakers?

The UVR suffixes and catalog numbers are as follows:
Volts AC        Suffix        Cat. #
24           UK           S29404  
48           UL           S29405  
110/130           UA           S29406  
208/277           UD           S29407  
380/480           UH           S29408  
525/600           UJ           S29409  
Volts DC        Suffix        Cat. #
12           UN           S29402  
24           UO           S29410  
30           UU           S29411  
48           UP           S29412  
60           UV           S29403  
125           UR           S29413  
250           US           S29414  

CTA-ID : 2062948
Was this helpful?
What can we do to improve the information ?