Technical FAQs

Ask a Question

What is the power supply voltage specification for the ATV312?

Voltage ranges are as follows:
200 - 15% to 240 + 10% for models ATV312....M2
200 - 15% to 240 + 10% for models ATV312....M3
380 - 15% to 500 + 10% for models ATV312....N4
525 - 15% to 600 + 10% for models ATV312....S6



CTA-ID : 2062610
Was this helpful?
What can we do to improve the information ?