Technical FAQs

Ask a Question

What is the remote keypad for the ATS22 soft starter?

VW3G22101 is an IP54 / Nema 12 keypad.
VW3G22102 is an IP65 keypad.
A cord is required to connect the keypad to the ATS22.  These are equipped with (2)RJ45 connectors.
VW3A1104R10 is 1meter ( 3feet ) long.
VW3A1104R30 is 3meters ( 9feet ) long.

CTA-ID : 2062614
Was this helpful?
What can we do to improve the information ?