Technical FAQs

Ask a Question

When replacing the Graphic keypad, VW3A1101, on an ATV drive, is any programming required?

No.  The program file resides in the drive.  When used with ATV61/71, there is the option to save the file to the keypad.


CTA-ID : 2062757
Was this helpful?
What can we do to improve the information ?