Technical FAQs

Ask a Question

On the ATV61/71, can FORWARD and REVERSE logic inputs be switched while the drive is running?

Yes.  When the direction is switched, the drive will ramp to a stop and then ramp up to the speed reference in the opposite direction.


CTA-ID : 2062377
Was this helpful?
What can we do to improve the information ?