Technical FAQs

Ask a Question

How is the ATV12 programmed to run via logic input on LI1 and adjust speed via dial?

Wire the run contact to +24 - LI1.
In the CtL menu, set Fr1 = AIV1, CHCF = SEP and Cd1 = tEr.
Press the dial twice to adjust speed as a percentage of the range LSP - HSP.

CTA-ID : 2062086
Was this helpful?
What can we do to improve the information ?