Technical FAQs

Ask a Question

Are the ATS48 keypads UV protected from direct sunlight?

The remote terminal VW3G48101 is delivered as a kit comprising:
- the keypad,
- a mounting kit containing a cover, screws and an IP 54 seal on the front panel to be positioned on the door of a floor-standing enclosure,
- a 3 m connecting cable (SUB_D9/RJ45).

The keypad itself is not UV protected, but the mounting kit uses a plastic material which is UV resistant.

Even though the mounting kit parts are UV resistant, note the following remarks:
- take care about the temperature (sunlight can warm up the keypad)
- direct sunlight on the screen display can reduce readability.


CTA-ID : 2062798
Was this helpful?
What can we do to improve the information ?