Technical FAQs

Ask a Question

ATV312 tripping on ObF fault.

If the drive trips while running, then check for power surges or spikes. Need to monitor for voltage surges and spikes. One may need to install a line reactor or a surge suppressor. If the drive is tripping while decelerating, then increase decelerating time. Optionally, add a Dynamic Braking resistor.
Was this helpful?
What can we do to improve the information ?