Technical FAQs

Ask a Question

ATV61 / 71 . Can I use a temperature sensor to control the drive speed?

No, the drive uses analog inputs. Temperature sensor output will need to be converted to voltage, current or a contact transistion (preset speed)


CTA-ID : 2062817
Was this helpful?
What can we do to improve the information ?