Technical FAQs

Ask a Question

Are the QO and Homeline Plug-On Neutral (PoN) load centers UL Listed?

Issue:
Load Center features

Product Line:
QO and Homeline Load Centers

Environment:
Codes and Standards

Cause:
Application

Resolution:
Yes, both the QO and Homeline Plug-On Netural(PoN) load centers are UL listed in the UL File E-6294.


CTA-ID : 2062749
Was this helpful?
What can we do to improve the information ?