Technical FAQs

Ask a Question

Do we offer a Type 3R, outdoor Plug-On PoN load center?

Issue:
Availability

Product Line:
Load Center

Cause:
Selection

Resolution:
Yes, some of the Type 3R QO load centers have been released with the PoN feature. 
All of the Type 3R Homeline load centers have been released with the PoN feature.
Refer to the latest online Digest for catalog numbers.


CTA-ID : 2062748
Was this helpful?
What can we do to improve the information ?