Technical FAQs

Ask a Question

Can Plug-On Neutral, PoN, CAFI or DF breakers be installed in standard QO load centers?

Issue:  
Plug-on Neutral arc-fault or dual function breaker will not install in QO load center.  

Product Line:
Residential load centers

Environment:  
QO Load Center

Cause:
Can the PoN plug-on neutral CAFI and DF breakers be installed in a standard QO load centers?

Resolution:
There is a rejection feature that will prevent the installation of the PoN CAFI and DF breaker in a standard QO load center.  The QO PoN CAFI and DF breakers are applicable only to QO Load Centers designed to accept them.  The Load Center catalog numbers will have a P in the catalog number suffix. 
Was this helpful?
What can we do to improve the information ?