Technical FAQs

Ask a Question

Does Square D offer Plug-On Neutral(PoN) CAFI branch circuit breakers for use in the HOMELINE load centers?

Product Availability

Product Line:
Homeline Load Centers

Branch Breaker Type


Yes, Square D does offer Plug-On Neutral(PoN), combination Arc Fault(CAFI) branch Breakers to be used ONLY in the new Plug-On Neutral Homeline load centers. The catalog numbers are HOM115PCAFI and HOM120PCAFI

NOTE: Square D also offers a Dual Function, Plug-On Neutral(PoN) branch breaker, with both Combination Arc Fault(CAF) and Ground Fault(GF) in a single branch breaker. The catalog numbers are HOM115PDF, HOM120PDF

CTA-ID : 2062745
Was this helpful?
What can we do to improve the information ?