Technical FAQs

Ask a Question

Do we offer 9001KN216 in plastic?

No the 9001KN200 and 9001KN300 legends are only available in aluminum.   This is because the lower half is so thin that it would break when it gets tightened down.  


CTA-ID : 2062215
Was this helpful?
What can we do to improve the information ?