Technical FAQs

Ask a Question

Can we get a 3/4`` hub in a 9001BR station?

Issue:
Can we get a 3/4`` hub in a 9001BR station?
Product Line:
9001B Standard Duty Control Stations
Environment:
30mm Control Stations and Enclosures
Cause:
Customer wants to clarify the conduit entry piping needed for application.
Resolution:
No, only ½ inch NPT is available.
Was this helpful?
What can we do to improve the information ?