Technical FAQs

Ask a Question

Does Schneider Electric offer a 240 V, 3 pole, 60A non-automatic molded case switch?

Yes we offer the QO300; the withstand rating is 10 kA.
Catalog number QO200 is a 2-pole switch with the same ratings.


CTA-ID : 2062362
Was this helpful?
What can we do to improve the information ?