Technical FAQs

Ask a Question

Are the standard and compact limit switch bodies like the 9007C54J considered watertight?

Yes, they are submersible down to 6 feet of water.   NEMA rating is 6P.  However, this rating is for submerging the switch without actuation.  Actuation under  water may allow water entry.  In addition, condensing of humid air within the body may result in water accumulation, as there are no drain holes.

CTA-ID : 2062167
Was this helpful?
What can we do to improve the information ?