Technical FAQs

Ask a Question

Can the ATS01 starter be installed after a contactor that only breaks 2 of the 3 phases to the motor?

No. All 3 phases must be made to the starter to soft start the motor. The contactor also needs an overload relay because the ATS01 does not provide motor overload protection.

CTA-ID : 2062039
Was this helpful?
What can we do to improve the information ?