Technical FAQs

Ask a Question

Can AP30210 and AP50210 be joined together?

Issue:
Can AP30210 and AP50210 be joined together? Will the two connect to each other?

Product Line:
Can AP30210 and AP50210 be joined together?

Environment:
Available 3 pole/3 wire wire Busway and a 3 pole/4 wire and existing Busway

Cause:
Can they be joined together

Resolution:
No. 3 Pole busway and 4 Pole busway systems are not compatible with each other. However, Schneider Electric can manufacture a special 3 Pole to 4 Pole transition device that would allow these two products to be connected. 








 

Was this helpful?
What can we do to improve the information ?