Technical FAQs

Ask a Question

What is the replacement part number for the ATS23PC24N?


Issue:   What is the replacement part number for the ATS23PC24N?
 
Product Line:   ATS23
 
Environment:  ATS23PC24N
 
Cause:   N/A
 
Resolution:   
 The replacement part number is ATS48C25Y.
Functionally the ATS48 can replace the ATS23 or ATS23P. There are some minor control and power wiring changes in certain applications.
Unlike the ATS23 or ATS23P, the ATS48 will require 110Vac or 220Vac Control power.
The dimensions are not all identical. Please refer to the ATS48 User`s guide 30072-450-61 for dimensional information.
Was this helpful?
What can we do to improve the information ?