Technical FAQs

Ask a Question

Is a wire harness included with the Two Programmable Contacts Module (M2C)? This is the cable that goes from the trip unit to the M2C.

Yes.
Was this helpful?
What can we do to improve the information ?