Technical FAQs

Ask a Question

Can the EasyPact breaker be reverse fed?

Yes, the EasyPact circuit breaker can be supplied from either the top or the bottom (reverse feeding) without any reduction in performance.
Note that this breaker does not have UL certification and is not sold or supported in North America.
Was this helpful?
What can we do to improve the information ?