Technical FAQs

Ask a Question

What are the dimensions and weights of the ATS48D62Y, ATS48D75Y, ATS48D88Y & ATS48C11Y?

These are all the same frame size.
Width = 7.48`` (190 mm)
Height = 11.42`` (290 mm)
Depth = 9.25`` (235 mm)
They each weigh 18.3 pounds (8.3 kg)


CTA-ID : 2061970
Was this helpful?
What can we do to improve the information ?