Technical FAQs

Ask a Question

EGB2HT and EGB3HT are listed in the Digest but are not valid numbers. Are they obsolete?


Issue:
Digest error in printed version 176

Product Line:
Circuit Breakers:

Environment:
Applies to ED, EG, and EJ handle ties.

Cause:
Handle tie requirement for ED, EG, and EJ circuit breakers.

Resolution:
No, just a misprint in the Digest (176, page 9-15, Table 9.60).  The correct handle ties for E-frame breakers are part number ECB2HT and ECB3HT.

Note: The Series 3 E-frame circuit breakers have been modified to accept the handle ties. This is the only modification from the previous Series 2 design.

** Handle tie kits may be applied to Series 3 E-frame circuit breakers only.
July 2010




CTA-ID : 2060337
Was this helpful?
What can we do to improve the information ?