Technical FAQs

Ask a Question

What are the components parts of the 600A mechanical main lug kit, part number NFCUM6 for an NF panelboard?

Verifying what parts are included with the NFCUM6.

Product Line:
NF panelboard.

Products sold in the United States.

Product features.

The component parts are:
(2) - neutral lugs
(2) A- and C- phase main lugs
(1) B- phase main lug assembly
(4) - 1/4-20 x 7/8-inch tapping screws
(6) 1/4 - 20 x 1-1/8 inch tapping screws

CTA-ID : 2058897

Was this helpful?
What can we do to improve the information ?