Technical FAQs

Ask a Question

What are the component parts that come with the mechanical main lug kit, part number NFCUM2 (250A) for NF panelboards?

Verifying what parts are included with the NFCUM2.

Product Line:
NF panelboard.

Products sold in the United States.

Product features.

The kit comes with the following:
(1) - neutral lug
(3) - main lugs
(1) 1/4-20 x 9/16-inch tapping screw
(3) - 1/4-20 x 3/4 inch tapping screws

CTA-ID : 2058895

Was this helpful?
What can we do to improve the information ?