Technical FAQs

Ask a Question

What is the load wire capacity of a NQNL2ACCY ?

Issue:
What is the load wire capacity of a NQNL2ACCY ?

Product LIne:
PTFDS - FD Enclosure Systems

Environment:
NQ panelboards and accessories sold and supported in the USA.

Cause:
Wire size for NQNL2ACCY accessory.

Resolution:
For either  Al or CU  wire :  1 #1/0 - 750kcmil or 2 - #1/0-350kcmil

















CTA-ID : 2055652
Was this helpful?
What can we do to improve the information ?