Technical FAQs

Ask a Question

How can you program the ATV212 Sflex to be reverse acting when using a 0-10V signal on VIB? They want 0V signal to be 60hz and 10V signal to be 0hz.

Programmed the drive as follows:
F210 - 0 %
F211 - 60.0 Hz
F212 - 100 %
F213 - 0.0 Hz
and wire your 0-10vdc signal to VIB and CC
Fnod needs to be 2


CTA-ID : 2062126
Was this helpful?
What can we do to improve the information ?