Technical FAQs

Ask a Question

What are the kit contents of the NQCUM2 main lug kit?

Issue:
What are the kit contents of  the NQCUM2 main lug kit?
 
Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker panelboards and accessories sold and supported in the USA.

Cause:
Listing of components of the NQCUM2 kit.

Resolution:
The NQCUM2 consist of the following parts:
(1)  Neutral mechanical lug
(3) Main mechanical lugs
(3)  1/4-20 x 7/8-inch tapping screws
(1)  1/4-20 x 9/16-inch tapping screws





















CTA-ID : 2059654
Was this helpful?
What can we do to improve the information ?