Technical FAQs

Ask a Question

XCSTE7311 and XCSTE7313: what are the differences?

The difference is in the conduit entry.  The ending 1 indicates metric devices tapped for 11 mm cable gland, conforming to NFC 68-300

The ending 3 indicates 1/2`` conduit entry and may be accomplished by a removeable adapter, or may be molded into the device.

For example: XCSTE5313 is electrically and functionally the same as XCSTE5311, differing only in threaded cable gland/conduit entry.


CTA-ID : 2061994
Was this helpful?
What can we do to improve the information ?