Technical FAQs

Ask a Question

What are the dimensions and weights for the ATV61HC22N4?

Width  =     440 mm       (17.32)   (in.)
height  =   1,190  mm   (46.62)   (in.)
Depth   =    350  mm     (13.78)    (in.)
Weight   =     163 kg       (358)   (lb.)


CTA-ID : 2062005
Was this helpful?
What can we do to improve the information ?