Technical FAQs

Ask a Question

Can the ATV61 or ATV71 be installed in an ATEX environment?

The ATV61 and ATV71 can be used in the functional safety loop for an ATEX application; however, they cannot be installed in the ATEX environment.  Only the motor can be installed in the ATEX environment.  Likewise, the remote keypad cannot be installed in the ATEX environment.


CTA-ID : 2061326
Was this helpful?
What can we do to improve the information ?