Technical FAQs

Ask a Question

What degree of protection is the Altivar ATV18 unit?

With the grey top on the unit it is rated IP31
WIth the grey top removed it is rated IP20


CTA-ID : 2062105
Was this helpful?
What can we do to improve the information ?