Technical FAQs

Ask a Question

What is included in the NQFTL4L and NQFTL4H 400A. Feed-Through Lug Kit?

Issue:
Verifying what parts are included with the NQFTL4L and NQFL4H.

Product Line:
NF panelboard.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
This kit contains the following parts:
(1) Neutral lug
(3) Feed-through lugs
(8) 10-32 x 5/16 in tapping screws
(2) 1/4-20 x 11/16 in tapping screws
(6) 1/4-20 x 7/8 in tapping screws
(2) Lug barriers
(2) Rail extensions
(2) Rail splices
(1) Cover extension

See instruction bulletin 80043-746-01 for step by step installation instructions.

CTA-ID : 2061465

Was this helpful?
What can we do to improve the information ?