Technical FAQs

Ask a Question

What is the ATV61 drives part number for a variable torque application like a fan or pump?


The ATV61 drives are rated to be used on light loads like Fan and pumps.  They range from 1HP up to 900 HP @ 480VAC 3phase,   1HP  to 125HP @ 230VAC 3 phase and 0.5HP to 7.5HP @ 230VAC 1 phase input 3 phase output.

See the attachment file for selection.
Was this helpful?
What can we do to improve the information ?