Technical FAQs

Ask a Question

Can both the Motor Frequency and Motor Current be monitored on the ATV212 display?

No, the display can only show one value at a time.  The same applies when using the VW3A1101 HMI or VW3A21101 remote display, only one option can be displayed.  


CTA-ID : 2061821
Was this helpful?
What can we do to improve the information ?