Technical FAQs

Ask a Question

What is the replacement contact kit for 8965DPR33?

Issue:
What is the replacement contact kit for 8965DPR33?
 
Product Line:
Class 8965 Contactors

Environment:
Definite Purpose Contactors

Cause:
Replacement Components

Resolution:
For Series B only customer can use 9998DRC3, which is a one pole kit.  Order quantity (6) to replace all poles of this reversing contactor.  


Series A and Series C devices do not have replacable contacts, as such the 9998DRC3 kit is obsolete.
 
Was this helpful?
What can we do to improve the information ?