Technical FAQs

Ask a Question

Is the 8736SCO7V02BS single phase or 3 phase?

It is 3 phase.  Refer to the current Digest for details.


CTA-ID : 2061850
Was this helpful?
What can we do to improve the information ?