Technical FAQs

Ask a Question

What is the difference between Micrologic trip unit types 6.0 and 7.0?

The 6.0 trip unit is for protection against major faults; the 7.0 is for earth leakage levels between .5 and 30A.  We don`t sell the 7.0 in North America and neither is designed for use with a resistance grounded system.

CTA-ID : 2061947
Was this helpful?
What can we do to improve the information ?